/content/sps/kr/ko/search-results.html
    Important Notice: 이 사이트는 5월 17일 일요일 오전 1:00 EST부터 오전 11:00 EST까지(5월 17일 일요일 05:00 UTC부터 15:00 PM UTC까지) 예정된 유지 관리가 진행됩니다. 이 기간 동안의 양해에 감사드립니다.

    Optimize the Performance of Your Critical Path for Operational Success

    A critical path is defined as a portion or subset of a material handling equipment (MHE) system and its associated components that are essential to the efficient and effective performance of a distribution and fulfillment (D&F) operation. Simply put, a critical path is a system or subsystem without which your operation simply cannot survive. A common example includes the coordination of sortation, induction, merge and accumulation conveyors. Performance optimization consulting (POC) is a targeted lifecycle management process through which an MHE vendor analyzes a critical path’s current operation and makes improvements to maximize its throughput and efficiency. This process starts by assessing the existing critical path’s MHE components. It includes a review of current business requirements (package sizes, throughput, customer service levels, etc.), conducts system-specific enhancements and improvements, and concludes by establishing a new performance baseline.

    Once the POC process is completed, internal maintenance and MHE vendors can then work to support this new performance baseline. This paper will detail a three-step POC process that can be used to deliver performance improvements on the most important system within a D&F operation.

    Download our white paper to learn exactly how these strategies can increase throughput in your operation.